Eaton
10000 Woodward Avenue
Woodridge, Illinois 60517
+1 773-869-1776
+1 (773) 869-1329
cpdipresaleshelp@eaton.com
United States
Contact Us

Burroughs Elementary School Protects Chromebooks from Theft with Eaton Charging Carts

Summary

Customer

John C. Burroughs Elementary School, serving approximately 500 students on the Chicago's southwest side.

Challenge

Following the theft of 30 iPads, new replacement Chromebooks need to be kept safe and secure during tight financial times.

Solution
CSC32AC
32-Port AC Charging Cart
A more feature-rich model is now available
CSC36AC
36-Port AC Charging Cart
Results

The school's new Chromebooks are being protected and charged by three Eaton Charging Carts. Students are able to enhance learning with technology at their fingertips once again.

About Eaton

Eaton is an intelligent power management company dedicated to improving the quality of life and protecting the environment for people everywhere. We are guided by our commitment to do business right, to operate sustainably and to help our customers manage power ─ today and well into the future. By capitalizing on the global growth trends of electrification and digitalization, we're accelerating the planet's transition to renewable energy and helping to solve the world's most urgent power management challenges.

Customer

John C. Burroughs Elementary School is a Chicago Public School serving approximately 500 students on the city's southwest side. The school's mission is to provide its students with a rich, holistic educational experience, leading them to become successful, independent and critical thinkers. Burroughs provides an academically rigorous and socially enriching environment where students are engaged through active and authentic learning.

burroughs elementary school

Illinois State Senator Antonio Muñoz joins Principal Richard Morris, along with Burroughs students and teachers as they prepare to place new Chromebooks in the Eaton Charging Cart.

Challenge

While neighborhood kids played during the school's weekend open gym hours, a thief slipped into a fourth-grade classroom and made off with 30 iPads used by students for learning.

Monday morning, teacher Maribel Herrera arrived at the school and discovered the tablets were missing. Herrera – and her students – were devastated by the loss. Budget cuts from the state of Illinois and the Chicago Public School System meant it would be difficult to buy new iPads. Burroughs administrators looked to the following school year to fund replacements.

When the new academic year and a new budget arrived, the school was able to procure enough Chromebooks to equip three classrooms. Meanwhile, administrators needed to find a solution to ensure the new Chromebooks would never meet the same fate as the pilfered iPads.

richard morris headshotThe Eaton Charging Carts are a great new addition to our classroom technology. Not only will the Chromebooks be protected from future theft, the carts give us flexibility for use and storage of the devices that we didn't have before.

Richard Morris
Principal, Burroughs Elementary School

Solution

csc32ac 32-port ac charging cart

32-Port AC Charging Cart

CSC32AC
  • Cart provides AC charging, secure storage and cord management for up to 32 Chromebooks and laptops up to 17 in. screen size
  • Locking steel doors and side panels prevent theft and tampering
  • Protective coated shelves with removable dividers and cord management keep devices organized
  • Flow-through ventilation prevents overheating during charging
  • Wide-grip handle and locking casters with non-marking wheels allow for easy maneuverability of devices across multiple classrooms

Results

Burroughs School acquired three of Eaton's AC charging carts. The new Chromebooks were recently delivered to the school and unveiled to the eager students. When not in use, the devices are stored and charged securely in the carts. And because the carts have smooth-rolling casters, it's easy to move devices between classrooms as needed. Principal Richard Morris is grateful Burroughs was able to acquire Chromebooks for the new school year and said the students are happy to have technology to help them learn at their fingertips again. "The students are thrilled to have the Chromebooks. This is the way kids learn these days. It's more natural for them," Morris noted. "And thanks to the Eaton carts, they will have technology in their hands for years to come."

Eaton charging carts in use

The new Charging Carts help students keep their Chromebooks organized at the end of the school day.

Need help with your purchase?
We're always available to help with questions, including product selection, sizing, installation and product customization. Call us at +1 773-869-1776 or email cpdipresaleshelp@eaton.com.